Corporate Blog

Stay curious. Real-world experiences.

Are you interested in the latest developments in drive technology? On the maxon blog, our experts report in detail on their work, new maxon products, and experiences from exciting collaborations.

Topics

  • R62_9957_Nn

    Young Engineers Program

    NTHU Racing x maxon: Driving Innovation on the Track

    A university racing team from Taiwan is taking on international Formula Student competitions with innovation and determination. This summer, they are heading to Europe to compete in Hungary, the Czech Republic, and Germany — aiming for a top-10 finish.
    Learn more
  • maxon Story

    The Circle Guitar: creating new kinds of music

    The Circle Guitar is a conventional electric guitar that hosts a spinning sequencer wheel, able to strike the strings at speed creating rhythms up to 300bpm and adding multiple layers of sound. This new instrument relies on a control and motion system that achieves precision in rhythm control. 
    Learn more
  • Newrotex harvests silk from Golden Orbweb spiders - 1maxon Story

    Spider silk spins new life into nerve repair

    Nerve damage is hard to repair and success rates are relatively low. But now, thanks to the advantages of spider silk, nerve repair has a much greater chance of success. Harvesting silk from live spiders involves a precise technique that demands an exacting drive system to control a low speed, highly accurate winding mechanism. 
    Learn more
  • Drone pilots will be able to quickly inspect and repair with AERASmaxon Story

    World’s first stable drone with robot arm to increase workplace safety

    A newly designed drone equipped with a six-axis robotic arm can maintain stability for precision tasks, such as maintenance and contact-based inspection. Launching this summer, the AERAS drone is set to reduce work at height accidents and speed up manual tasks. 
    Learn more
  • ECX_PRIME_6_cutmaxon Story

    maxon expands high-torque, high-speed BLDC motor range

    Precision drive system manufacturer maxon has expanded its high speed and high torque brushless DC (BLDC) motor series to extend capabilities for applications that demand a compact footprint and low weight. The new 22mm diameter BLDC motor in maxon’s ECX PRIME series increases nominal torque to 69.1mNm with high-speed operation up to 30,000rpm. ECX PRIME motors feature a rigid speed-torque characteristic that optimises control for precision applications.
    Learn more
  • Image2maxon Story

    Motorized Precision in Pipelines

    Deep underground, where light fades and sludge builds up, robots are taking on the dirty work—and a Swiss drive system is powering their precision
    Learn more
  • software-programmingExpert Blog

    maxon multi-axis motion controller now in motherboard integration format

    maxon’s MicroMACS6 multi-axis motion controller is now available in a PCB module format for integration with custom-designed motherboards. 
    Learn more
  • maxon - Multi-axis motion control is required for pipe inspection robotsmaxon Story

    Multi-axis motion control drives pipe-based robots

    Surveying and maintaining underground pipes can be complex and resource intensive. To streamline the process, construction and facility management teams are increasingly turning to robots that can provide inspection as well as repair. 
    Learn more
  • colossus-207f3544maxon Story

    A "Swiss Army knife" robot – powerful, reliable, and robust

    To disinfect surfaces without taking risks, the Bataillon de Marins-Pompiers (marine fire service) from Marseille has equipped itself with two Colossus robots. These remote control and highly modular autonomous robots are proving to be valuable assets in the fight against Covid-19. 
    Learn more
GettyImages-1461120258

Media Center

Even more stories and publications.

In the maxon Media Center we present more exciting stories from the maxon universe. Here you have access to publications such as product brochures, and current and archived issues of our customer magazine. Many publications are also available for download.

Learn more