maxon motor takes part in chase to catch up with a comet

Rosetta mission

After more than ten years of travel through space, the European space probe Rosetta has reached the comet Chury. Three months from now, for the first time in the history of space travel, a lander will touch down on the surface of the four-kilometer-wide comet. DC motors manufactured by maxon are part of this pioneering feat.

  • On August 6, the big day came: After a journey of more than ten years, the Rosetta space probe reached the comet 67P/Churyumov-Gerasimenko, known as “Chury” for short

    The Philae lander is scheduled to touch down on comet 67P in November. © 2014 ESA/Rosetta/NAVCAM

On August 6, the big day came: After a journey of more than ten years, the Rosetta space probe reached the comet 67P/Churyumov-Gerasimenko, known as “Chury” for short. The mission team at the European Space Agency (ESA) jumped for joy. For the first time in the history of space travel, a probe has rendezvoused with a comet. It will now orbit and map the comet and gather various types of data. Already, the first images received have yielded astonishing new insights: The comet Chury, which is four kilometers wide, is not round or oval, but instead looks like two rocks loosely stuck together. At minus 70 °C, the surface is much warmer than expected and the first information indicates that it is covered with a black layer of dust.

First choice for space missions
Rosetta will now gradually approach the comet, until a distance of only 10 kilometers separates them. The most difficult part of the mission will take place in mid-November 2014, when the Philae lander is scheduled to touch down on Chury. It will be the first controlled landing on a comet. A real pioneering feat - and maxon motor is part of it, with a DC motor on board. This is not the first time that the micro drives from Switzerland have been the first choice for space missions. SpaceX's Dragon spacecraft, which transports cargo to the ISS station, also contains maxon motors. The same holds true for the Mars rovers, which have been diligently traveling across the surface of the red planet for many years.

What is next? On our Twitter channel @maxonmotor, we will keep you up-to-date with news from the Rosetta mission.

Back to the news overview

Contact

maxon motor ag

Brünigstrasse 2206072 SachselnSwitzerland
+41 (41) 666 15 00
Contact