Media Release 03/25/2019

More drive power on all levels.

ID156_XL_24V_A-Flange
IDX compact drive with integrated EPOS positioning controllers and IP-protected housing. ©maxon motor ag

maxon will show the latest in drive technology at the Hannover Messe.


Drive specialist maxon motor will be presenting exciting new products at the world's largest technology trade show. Some new products being featured include: flat motors with improved performance, a new line of modular industrial drives, as well as DC motors and angular gearheads from Parvalux, the latest addi-tion to the maxon group.

ID156_XL_24V_A-Flange
EC90_flat_500W_Back
ID156_XL_24V_A-Flange
EC90_flat_500W_Back

IDX compact drive with integrated EPOS positioning controllers and IP-protected housing. ©maxon motor ag

1/2

Powerful drives, high power density and easy integration — these keywords best describe this year's presence at the world's largest technology trade show in Hanover from April 1st – 5th. maxon motor will present new solutions that will benefit customers all over the world.


Special attention should be paid to the new IDX line, a modular drive system for applications in industrial automation or logistics automation that consists of a motor and an integrated EPOS4 controller that can be used in a wide varie-ty of applications. The IDX compact drives will be configurable online.

 

Solutions with no performance limits


Parvalux will be making a special appearance at the maxon stand this year. The established UK company has been part of the maxon group since the beginning of the year and expands the product portfolio with DC and AC mo-tors up to 1.5 kW as well as suitable angular gearheads. These are used for a wide variety of applications, from stair lifts to transport systems and industrial robots. maxon CEO Eugen Elmiger comments: “We will no longer have an upper performance limit in the future.”


maxon has also boosted the performance of its popular brushless flat motors (with diameters of 60 and 90 millimeters): A new design has resulted in signif-icant performance increases of up to 100 percent. Both the EC 60 flat and the EC 90 flat drives are now available as power-up versions, either with an open rotor or with an attached fan. As a result of optimal motor cooling, the EC 60 flat now delivers 200 W of power, while the EC 90 flat achieves 600 W. The flat motors are particularly suitable for applications where space is limited but high drive power is needed. Some logistics applications include, belt drives or autonomous vehicles.


In addition, maxon will present further innovations such as the ENX EASY XT encoder for use in harsh environments, or the tiny brushless ECX Speed with a diameter of 6 millimeters, which can be configured online like all of the other X drives. For more information please visit: shop.maxonmotor.com


maxon will have two booths at the 2019 Hannover Messe:

  • Hall 15, booth D09 (Industrial Automation)
  • Hall 3, booth N03 (Industrial Supply/maxon ceramic)
     

© by © maxon motor ag