maxon Story

AGVs: The solution in logistics?

Topics

Template DriveTech 1500x1000 agv logistique3Template DriveTech 1500x1000 agv logistique3

AGVs (automated guided vehicles) are essential tools in the current commercial and industrial transformation. But what challenges do they need to address?


The AGV market: why are we seeing such a boom today?


Back in the 1950s, car manufacturers used guided vehicles in their factories to distribute mechanical parts. Since then, different methods have been developed to move these motorized robots on demand. There are now around half a dozen technologies used in these vehicles today:


•    self-guided
•    line-guided
•    opto-guided (by lines marked on the ground)
•    geo-guided
•    laser guided
•    or even guided by ultrasound.

All of these are now grouped under the AGV umbrella. This market currently represents EUR 550 million, primarily within Europe, and could reach EUR 1.35 billion by 2023. Its rapid growth is due in particular to e-commerce companies, where the technology is developing exponentially. Therefore their priority is to continually optimize their internal logistics processing in order to organize the company and ensure increasingly fast deliveries. Amazon was one of the first to integrate AGV technology by creating its own smart vehicles. Manufacturers are also using this method in their automated warehouses, where AGVs address the issue of compact size in particular.


These intralogistic robots are also being used more and more in the area of goods-to-person logistics, where AGVs transport objects and heavy loads directly to human workers. This way of working is known as cobotics – a collaboration between humans and robots. And AGVs provide an optimized response by taking over strenuous and repetitive tasks.


Why do AGVs provide the perfect answer to challenges in logistics?


With the development of e-commerce, logistics services now need new solutions. AGVs address all the challenges that arise within a distribution chain:


•    First and foremost, they increase productivity, speed and quality by allowing the operators to process larger volumes of goods, all while offering reliability. This approach is more than 30% faster compared to humans working alone, and there are fewer errors. Therefore companies are able to consistently fulfill their orders more quickly, and at the same time offer greater safety for people and goods.


•    AGVs enable better working conditions with their mechanical assistance, which helps to significantly reduce musculoskeletal disorders (MSDs) and accidents in the workplace. This is the overall purpose of cobotics (collaborative robotics): the cobots alleviate physical discomfort in human workers without preventing them from performing their activities.


•    They also enable space savings in warehouses due to better organization and optimization of space. This offers a huge real estate advantage at a time when every square meter saved represents a financial gain over several years.


In terms of production, the return on investment can be seen over one or two years.

Template DriveTech 1500x1000 agv logistique


Manufacturers/designers of AGVs: what are the technical constraints and challenges of the sector?


Before being able to address the needs of their customers, in logistics especially, manufacturers have to tackle the technical constraints. AGVs must offer long-term reliability and robustness so they can function without any need for maintenance for at least two years in order to optimize the profitability of warehouses. Bear in mind that any downtimes result in a chain reaction that can lead to huge financial losses.


•    See also: The 5 essential points for motorizing an AGV

AGVs must also be compact to allow their owners to occupy smaller warehouses and lower their operating costs. Smaller yet still capable of transporting heavy loads, AGVs must offer substantial power density. The challenge of miniaturization for space savings and drive systems  for efficiency and robustness is therefore fundamental.

Template DriveTech 1500x1000 agv logistique2


maxon – serving AGV manufacturers and designers


Optimizing space


maxon develops compact motors offering high torque and speed density, such as EC Flat and ECi. These compact motors also consume less energy than other products on the market. This is a powerful argument for manufacturers that need to reduce their costs and address the challenges imposed by energy transition.


Operating efficient communication buses


To address maintenance challenges, the motors with integrated electronics installed in the AGVs must be network-connected. The communication buses of motors from the IDX range are able to communicate simultaneously with the EtherCAT and CANopen systems and on IoT networks. Therefore, these robots can be programmed by computer and operated remotely, meaning that a single intervention is required to control the entire fleet of AGVs.


Specific mechatronic developments


Compact size, multi-axis systems, power density, specific protection ratings… Depending on your project, there are multiple requirements and finding adapted mechatronic solutions is not always easy. From defining the specifications to designing the products, maxon’s specialist mechatronics team supports you by providing sound knowledge and expertise in the development of customized projects. Our technicians remain available following implementation to deliver ongoing technical support. Contact our mechatronics experts.


In order to offer AGV designers maximum freedom, the maxon Group has developed an entire range of compact and modular motors. These IDX drive solutions meet the most demanding requirements: offering 20% higher performance compared with the current solutions on the market, the safe, modular and easy-to-configure motors meet all your drive needs.

Template DriveTech 1500x1000 agv top3 des secteurs porteurs5

To find out more about the IDX, visit idx.maxongroup.com
Author: Madeline Vassaux