maxon Story

Minimally invasive surgery.

Topics

Template drivetech 1500x1000 keyhole surgery robotTemplate drivetech 1500x1000 keyhole surgery robot

The Bristol Robotics Laboratory is incorporating maxon products as part of a project to develop Robot Assisted Minimally Invasive Surgery (RAMIS).

Minimally invasive keyhole surgery assisted by robots

Using robots in minimally invasive keyhole surgery offers many advantages compared to traditional minimally invasive surgery, including improved vision, precision, and dexterity. The SMARTsurg project has been set up to develop an advanced system for performing robot-assisted MIS.

The project involves a team of ten institutions across Europe of highly experienced clinical, academic, and industrial partners. One of the institutions is the Bristol Robotics Laboratory (BRL). maxon has worked with BRL on several projects and was delighted to be asked to assist on RAMIS.

The team is using maxon DC motors and controllers to drive and position the 3-finger surgical instrument that goes inside the body. The instrument will be controlled by exoskeletons that fit over the surgeon’s hands. In addition, they are also developing smart glasses to allow the surgeon to have a realistic view of what is taking place inside the body. The team found maxon products were easy to use and offered the precision and high power density necessary for this application.

BRL used the maxon online Configurator to select and configure the DCX 19 S brushed DC motor, the GPX 22 gearhead, and the ENX 10 encoder. An advantage of using the maxon Configurator is the short lead times.

Designing the maxon products online enabled the best fit package in terms of output torque, speed, and encoder feedback. Physical dimensions could also be realized at the touch of a button, simply and quickly including full technical details of the package published, including a 3D CAD model. The maxon EPOS2 positioning controller and the CAN communication protocol were used to ensure each axis responds to commands from the master controller in terms of position, speed, and torque.

“While the popularity of RAMIS is steadily increasing, the potential for improving patient outcomes and the potential for other procedures are not fully realized”

Sanja Dogmadzi, professor in Medical Robotics at BRL explained, “While the popularity of RAMIS is steadily increasing, the potential for improving patient outcomes and the potential for other procedures are not fully realized, largely because of serious limitations in the current instrumentation, control, and feedback to the surgeon. Specifically, restricted access, lack of force feedback, and use of rigid tools in confined spaces occupied by organs pose challenges to full adoption.” 

The development of robotic surgical platforms has introduced 3D vision and significant improvements in the levels of dexterity. Robot-assisted minimally invasive surgery will reduce the demand on the surgeon, shorten training time, and deliver accuracy, safety, and reduced procedure time.

Author: maxon France

© by © maxon motor ag