maxon Story

Inside the Future of Industrial Robotics

Topics

Armatrix2EC-frameless_DT50M

Behind steel walls, beneath ship decks, and deep within industrial vessels, a new generation robot is quietly redefining how critical assets are inspected, maintained, and protected by Swiss precision.

India's industrial sector is undergoing rapid modernization. From expanding shipbuilding capabilities and strengthening port infrastructure to scaling heavy manufacturing and energy operations, industries are under increasing pressure to improve efficiency, safety, and asset reliability.

Initiatives such as Make in India, increased investments in industrial automation, and the push towards globally competitive manufacturing are accelerating the adoption of advanced robotics and intelligent maintenance technologies. At the same time, industries continue to face challenges associated with aging infrastructure, labor-intensive inspections, and hazardous maintenance environments.

This is where Armatrix is bringing a fresh perspective.

Inside The Future of Industrial robotics

Founded in 2024, by IIT Kanpur alumni in India, Armatrix is on a mission to solve one of industry's most persistent challenges: enabling safe access to spaces that are difficult, dangerous, or impossible for humans to enter.

What Armatrix is Building

At Armatrix, the goal is not simply to build another robotic arm. The company develops snake-like compact, cable-driven robotic arms designed to navigate complex industrial environments while supporting critical inspection and maintenance operations

This creates a unique set of engineering challenges.

The robotic architecture demands motors with high power density in an extremely compact form factor, because every joint must generate sufficient force without adding unnecessary size or weight. In confined spaces, even small increases in joint dimensions can reduce maneuverability and limit access to critical areas.

Maintaining stiffness presents another challenge. Cable-driven systems are highly efficient and lightweight, but cables can stretch and experience changing tension during operation. Without precise control, this can affect positioning accuracy and repeatability, two critical requirements for inspection and maintenance tasks.

As a result, the system requires:

  • High-frequency encoder feedback
  • Fast and precise corrective motion
  • Responsive closed-loop control
  • Continuous monitoring of joint position and cable tension

These requirements place exceptional demands on the drive system and motion-control architecture.

Why maxon?

For Armatrix, motion performance is not just a specification. It is fundamental to the robot's ability to operate reliably in real-world industrial environments.

This is where maxon EC motors, gearboxes and EPOS4 controllers play a critical role.

maxon provides the compact actuation, high-speed responsive closed-loop control, and advanced diagnostic capabilities needed to continuously regulate joint position and cable tension. The combination enables Armatrix to enhance stiffness, improve positioning accuracy, and increase overall system reliability while accelerating the development of its multi-joint robotic platforms.

The partnership illustrates how precision drive technology can directly influence robotic performance at the system level.

EPOS4-Compact-24-5
EC-frameless_DT50M
maxon -GSW A strainwave gear - exploded view
EPOS4-Compact-24-5
EC-frameless_DT50M

EPOS4 Compact 24/5 EtherCAT 3-axes

1/3

Reinventing Robotics for Confined Spaces

The Armatrix robotic platform stands apart from traditional industrial robots.

Its snake-like structure allows it to enter through small access points and navigate intricate internal geometries that would be inaccessible to conventional robotic arms. This flexibility enables inspection and intervention without requiring extensive asset disassembly or structural modifications.

A key differentiator is Armatrix's external actuation architecture, where drive mechanisms are located outside the arm body. By separating the actuation system from the arm itself, the robot can operate in environments with moisture, contamination, hazardous gases, or extreme temperatures where internal electronics may be vulnerable.

The platform can be equipped with a variety of end-effectors for:

  • Visual inspection
  • Non-destructive testing (NDT)
  • Welding
  • Painting and coating applications

This modular approach allows a single robotic system to perform multiple maintenance functions, improving efficiency and reducing deployment complexity.

A Strong Fit for India's Industrial Future

India's push toward advanced manufacturing, industrial automation, and world-class infrastructure is creating demand for technologies that improve both safety and productivity.

Industries such as:

  • Shipbuilding and ship repair
  • Oil & Gas
  • Power generation
  • Steel manufacturing
  • Chemical processing
  • Ports and maritime infrastructure

All face challenges associated with confined-space inspection and maintenance.

As organizations pursue smarter maintenance strategies and Industry 4.0 initiatives, robotic solutions capable of operating where humans cannot become increasingly valuable. Armatrix's innovative robotic architecture, combined with maxon's precision drive technology, offers a compelling solution to these challenges.

Together, we are helping industries move toward a future where critical inspections and maintenance operations can be performed more safely, more efficiently, and with greater confidence than ever before.