Media Release 04/11/2024
maxon presents a humanoid robot and current product highlights at SPS 2024
At the SPS 2024 trade fair in Nuremberg from November 12 to 14, maxon will present the first complete prototype of the humanoid robot HOPE. HOPE is driven by maxon EC-i motors and the company's own controllers. Rob Knight, the developer of the robot, will be present at the maxon booth throughout the trade fair. maxon will also be showcasing current highlights from its product range, including the new "Strain Wave" shaft gearhead, which will be making its trade fair debut.
Drives for robots are an important business segment for the maxon Group. maxon develops and manufactures customised components for autonomous mobile and industrial robots, including humanoid, four-legged, collaborative, or agricultural and service robots.
The prototype of the humanoid robot HOPE shows how maxon drives are used in robotics in a very practical way. This will be on display with its developer Rob Knight from "The Robot Studio" at the maxon stand at SPS in Nuremberg. With a height of two metres and the ability to move freely and keep its balance for up to an hour, HOPE offers exciting insights into its functionality. Visitors can interact with HOPE on-site.
HOPE can move thanks to maxon drives. Four EC-i 40 drives are used in each of the arms. These are brushless motors with an iron-core winding and internal rotor, which develop high dynamics and high torques in the smallest of spaces. Six EC90 flat motors are also installed, which deliver high torques even in confined spaces. The drives are controlled by maxon EPOS4 position controllers.
Rob Knight and his HOPE robot can be seen from November 12 to 14 at SPS in Nuremberg, Hall 3, Stand 260.
Other product highlights that maxon will be presenting at the SPS:
Drives: on display, in addition to the EC-i 40 described above, are the following drives: High Efficiency Joint 90 (an extremely compact, integrated and efficient robot drive system that contains all subsystems for a complete motion solution, e.g. electronics, motor, gearhead and sensors); ECX Prime 6 and 16 (brushless BLDC motors with high torques at high speeds) and the ECX Flat 22, 32 and 42 (flat motors with external, multi-pole rotor, particularly suitable for limited space).
Gearheads: maxon will be premiering the new "Strain Wave" gearhead, which will be available from next year and stands for high precision and compactness .
Controllers: With ESCON2, maxon is presenting the further development of its proven controller product line, which is now also available for highly miniaturised applications. The MicroMACS6, the freely programmable and ultra-compact multi-axis motion controller, will also be on show.
Further highlights: The heavy-duty motors from Parvalux by maxon, technical ceramics and the maxon e-bike drive BIKEDRIVE AIR will also be on display.
Further information
For further information, please contact Lena Gulder, Marketing Manager maxon Germany:
Phone +49 89 420 493-59
lena.gulder@maxongroup.com