Corporate Blog

Stay curious. Real-world experiences.

Are you interested in the latest developments in drive technology? On the maxon blog, our experts report in detail on their work, new maxon products, and experiences from exciting collaborations.

Topics

  • Newrotex harvests silk from Golden Orbweb spiders - 1

    maxon Story

    Spider silk spins new life into nerve repair

    Nerve damage is hard to repair and success rates are relatively low. But now, thanks to the advantages of spider silk, nerve repair has a much greater chance of success. Harvesting silk from live spiders involves a precise technique that demands an exacting drive system to control a low speed, highly accurate winding mechanism. 
    Learn more
  • Drone pilots will be able to quickly inspect and repair with AERASmaxon Story

    World’s first stable drone with robot arm to increase workplace safety

    A newly designed drone equipped with a six-axis robotic arm can maintain stability for precision tasks, such as maintenance and contact-based inspection. Launching this summer, the AERAS drone is set to reduce work at height accidents and speed up manual tasks. 
    Learn more
  • ECX_PRIME_6_cutmaxon Story

    maxon expands high-torque, high-speed BLDC motor range

    Precision drive system manufacturer maxon has expanded its high speed and high torque brushless DC (BLDC) motor series to extend capabilities for applications that demand a compact footprint and low weight. The new 22mm diameter BLDC motor in maxon’s ECX PRIME series increases nominal torque to 69.1mNm with high-speed operation up to 30,000rpm. ECX PRIME motors feature a rigid speed-torque characteristic that optimises control for precision applications.
    Learn more
  • maxon - Smart ergonomic chair - 2Young Engineers Program

    Academic projects designed for the real world

    Academic engineering projects not only help create the design minds of tomorrow, but the resulting creations often achieve innovation in their own right. The University of Bath’s Mechanical Engineering Department fosters this spirit, partnering with supporters from industry to innovate for the real world.
    Learn more
  • software-programmingExpert Blog

    maxon multi-axis motion controller now in motherboard integration format

    maxon’s MicroMACS6 multi-axis motion controller is now available in a PCB module format for integration with custom-designed motherboards. 
    Learn more
  • maxon - Multi-axis motion control is required for pipe inspection robotsmaxon Story

    Multi-axis motion control drives pipe-based robots

    Surveying and maintaining underground pipes can be complex and resource intensive. To streamline the process, construction and facility management teams are increasingly turning to robots that can provide inspection as well as repair. 
    Learn more
  • images-dt-flybotix-update-header-9f669504maxon Story

    Challenges in Drone Technology

    Drone technology continues to advance depending on specific applications. For this article, we’ll be looking at compact drones used in a variety of applications that need continuous and autonomous inspection of chimneys, shafts, and tanks.
    Learn more
  • header-autonomous-2400x1600-dt-400efb74maxon Story

    Robots speeding up material handling

    With omnidirectional movement and smart docking with virtually any warehouse cart in under 20 seconds, these new robots are making material handling faster and safer.
    Learn more
  • photo_6-84b1cf7fmaxon Story

    New era for Maritime Autonomous Surface Ships

    maxon Drive System Opens an Era for Maritime Autonomous Surface Ships (MASS). Providing a High Level of Reliability and Swift Custom Service on One of the World’s Largest Container Carriers.
    Learn more
GettyImages-1461120258

Media Center

Even more stories and publications.

In the maxon Media Center we present more exciting stories from the maxon universe. Here you have access to publications such as product brochures, and current and archived issues of our customer magazine. Many publications are also available for download.

Learn more