maxon Innovation

«Drive system specification is crucial when precision matters»

Topics

maxon - Aviation is an important sector for maxonmaxon Drive Technology Insight 2024 - (14) - maxon MD Will Mason in drive technology discussion

Providing the motion for applications ranging from robotics through to medical implants, demands on the precision drive system market continue to include closer control and more compact designs. This trend is increasing the emphasis on the concept development stage. maxon UK & Ireland’s Managing Director, William Mason, explains how engineering support in the drive system market has developed – and where it’s going.

Over the past 25 years, the precision drive system market, involving DC and brushless DC motors up to around 750W, has continued to develop progressively compact, torque-dense systems, with greater control. These advances have enabled design engineers to specify electric drive systems, also comprising gears and controls, that are increasingly specific to task. 

“The biggest change in drive system development has been the complexity of projects, including modifications to create completely bespoke motors,” says William Mason, Managing Director of electric drive system manufacturer, maxon UK & Ireland. “20 years ago, modifications might have involved a customised shaft or a cable change. Today, drive systems can be designed from scratch. Instead of the customer fitting their needs around what is available, now drive systems are designed to fit customers’ exacting requirements.”

Applications where performance is the most critical have benefitted the most. This has changed the market focus for precision drive system manufacturers like maxon, where high-volume OEMs require custom development. 

“Today, our biggest market in the UK is aerospace, followed by the medical sector, which is growing fast thanks to developments such as patient-implantable devices,” says William. “The continued growth of robotics, with use spreading across more and more sectors, is also important.” 

The demand for customisation

The ability to develop a customised drive system is dependent on the experience and expertise of the engineers responsible for specification. This role has become increasingly important as application needs have become more demanding.

William Mason, Managing Director maxon UK & Ireland

«Drive system manufacturers are likely to become more involved with software programming for controllers.»

“Today, design engineer customers frequently provide a detailed specification of requirements. As a result, it’s crucial for locally based, front line engineers to carry out a detailed review and create an accurate design concept. Getting that stage right is essential for the R&D and manufacturing teams to develop a drive system that best achieves the neds of the application,” says William. 
Responding to the shifting demand for customised development, maxon has invested in its UK & Ireland engineering team to support customers in drive system specification. 

“All of the team, including myself, have engineering degrees as well as backgrounds in engineering. When we talk to a customer about their application, our team understands the requirements on the drive system and the possibilities in customisation that can be achieved,” adds William.

This knowledge extends into specialised sectors where distinct demands are supported by a top-down approach that spans R&D, material sourcing, and manufacture. 

Developing complete drive systems

“Particularly for sectors where motor performance is critical, industrial standards are now commonly applied, covering component and material traceability, design criteria, as well as production. Recognition of EN ISO certifications for the medical and aerospace industries, for example, have been crucial for drive system manufacturers to achieve,” says William.

maxon Drive Technology Insight 2024 - (14) - maxon MD Will Mason in drive technology discussion
maxon MD Will Mason in drive technology discussion.

The push for standards has coincided with the trend for complete drive system development, rather than providing the motor-only. This includes the gear head, feedback device, a controller for speed, torque, and position, and if necessary, a controller to coordinate multiple axes. 
“Design and assembly of a drive system can reduce development time for the OEM or project engineering team. Most importantly, relying on a dedicated engineering team to develop a turn-key drive system can increase performance for real world use,” says William. 

Since the 2018 acquisition of the Poole-based motor manufacturer, Parvalux, this has widened maxon’s capabilities, adding right-angle geared motors, higher power AC systems, as well as DC motors for consumer and industry-scale markets. The partnership has also enabled combined technology projects, such as pairing a flat, brushless DC maxon motor with a Parvalux right-angle gearbox to create a compact, automated door control system. 

Future market demands in precision drive systems 

Concentrating on the core market of precision drive systems, how will customer requirements push developments in future? 
“Drive system manufacturers are likely to become more involved with software programming for controllers, as we continue to see the developing need for complete, turn-key systems,” says maxon UK & Ireland’s Managing Director. “The DC motor itself has been around for a very long time and it won't fundamentally change. However, we will see improved tolerances and magnet strength, creating more powerful motors for their size. Today’s primary need for precise, compact, and highly reliable drives will be even more in demand in future as OEM’s look to increase the performance and efficiency of their systems.” 

maxon’s £603million annual turnover is led by its American customers with a very strong medical market, followed by Germany and home customers in Switzerland. The UK and Ireland will continue to be important for the precision drive system market thanks to the requirements of its high-tech industrial base, particularly including the medical, automotive, and aviation sectors. While large OEMS lead maxon UK & Ireland’s turnover, the formation of its own drive system engineering team, set up 25 years ago, has enabled the company to support start-ups and academic projects that have grown into significant businesses.

maxon ECX Multi Pole
maxon ECX flat motor
maxon - SCARA robot joint actuator - robotics continues to be a growing sector
maxon ECX Multi Pole
maxon ECX flat motor

maxon ECX Multi Pole

1/3

“One of our top 10 customers started out as a university project. They developed a process 20 years ago and turned it into a business. We’ve been supporting them ever since,” says William. “We never know how successful start-up businesses or university projects could eventually become. That potential for growth is one of the reasons we’re keen to support them.”

Whatever the scale, the success of future projects involving precision drive systems will continue to rely on first-hand engineering expertise from outset. The higher the demands on the drive system, the more important that initial design concept will become. 

Author: maxon UK