2_Autonomous Mobile Robot AMR with maxon Wheel Drive

Media Release 18/11/2026

maxon at SPS 2026: Functional safety for robotic joints and solutions for autonomous systems

At SPS trade fair 2026 in Nuremberg, from November 24 to 26, 2026, maxon will present new products for robotics and industrial automation. The focus is on new drive solutions, functional safety, and intelligent technologies. At our booth, maxon's system expertise will be demonstrated through the example of an autonomous mobile robot (AMR) – from individual components to integrated drive systems and engineering and predictive maintenance.

The demands for modern automation solutions are increasing: compact, powerful drives are in demand that can be easily integrated while meeting the highest standards of safety and reliability. For this reason, maxon continuously expands its portfolio of solutions with functional safety. Good examples of this are the High Efficiency Joints for robotics and the industrial drive IDX. Both demonstrate how powerful drive technology and safety functions can be integrated into modern machine and robot concepts.

maxon has also further developed its trade fair appearance. The booth offers visitors new opportunities not only to get to know technologies and products but also to experience them interactively. An autonomous mobile robot (AMR), as used for example in logistics, forms the connecting element. Using this concrete application, maxon demonstrates the interplay of its expertise: from motors, gearboxes, and controllers to complete drive systems like the maxon Wheel Drive and custom engineering solutions, all the way to intelligent functions. This also includes maxon MIND, the predictive maintenance platform that uses condition data to detect maintenance needs early. This clearly shows how maxon supports its customers far beyond the delivery of individual drive components.

Product innovations and highlights at the maxon booth

  • High Efficiency Joints with Functional Safety: maxon's High Efficiency Joints are an established and scalable platform of highly integrated quasi-direct drives for modern robotics. They are already used in humanoid robots, four-legged robots, and manipulators. With the new variant with functional safety, maxon expands the platform with integrated safety functions without compromising on size or system integration. The drives remain backward compatible with existing High Efficiency Joints and offer features such as Safe Limited Torque, which are especially relevant for manipulation tasks. This lays the foundation for future requirements for safe and dynamically balancing robot systems.

  • ESCON2 controller now offers positioning: The servo controllers of the ESCON2 family receive a new function: With a free firmware update, the existing hardware becomes a CANopen positioning controller. Among the supported modes are Profile Position, Cyclic Synchronous Position, and Homing. The holding brake can also be controlled directly via the drive. The update will be available from December 2026 and allows existing ESCON2 drives to be upgraded without hardware changes. The ESCON2 platform includes nine variants from Nano to Compact and is suitable for a wide range of applications, from laboratory automation and optics to AGVs and logistics.

  • Frameless portfolio expanded: maxon continues to expand its product families of frameless motors. The EC frameless Dynamic Torque family now includes four diameters. The high copper content enables high torque density and dynamic performance. Integrated Hall sensors require no additional installation space in the motor length, while a large hollow shaft provides space for cables and other integration elements. The portfolio is complemented by the EC frameless High Torque. It offers a cost-effective alternative for applications with higher production volumes and limited budgets.

  • New sizes in maxon’s strain wave gearheads: The range of strain wave gearheads is also growing: new compact sizes with diameters of 20, 30, 40, and 70 mm expand the range of applications. The backlash-free gearheads enable highly precise positioning with high torsional stiffness and repeatability.

Visit us at SPS 2026: Hall 4, Booth 239

Experience maxon's drive solutions in combination and discover how complete, intelligent systems can be developed from individual components. Our experts look forward to meeting with visitors and exchanging ideas.

More information

For further information, please contact Lena Gulder, Marketing Manager maxon Germany: 

Phone +49 89 420 493-59

lena.gulder@maxongroup.com

Images

Images related to this announcement can be downloaded by clicking the download button of this announcement. The images may only be used in connection with reporting about maxon.

About maxon: The Swiss specialist in quality drives

maxon is a leading supplier of precise electric motors and drive systems, developing drive solutions tailored to the needs of customers in medical technology, industrial automation, aerospace, mobility, and robotics. Founded in 1961, the Swiss company is owned by the Braun family and is headquartered in Sachseln (OW). The maxon Group employs around 3,400 people worldwide at tenproduction sites and is present in over 40 countries.