Expert Blog

MiniMACS6 stabilizes the Furuta pendulum.

Topics

DT 1500x1000 zub_MiniMACS6-AMP-4-50-10_ohne_EthernetDT 1500x1000 zub_MiniMACS6-AMP-4-50-10_ohne_Ethernet

A classic problem in engineering is the rotational inverted pendulum. It is used to demonstrate and examine movement patterns and control algorithms in control and electrical engineering as well as in mechanical engineering. These help to control robots and other machines.

The pendulum, named after its Japanese inventor Katsuhisa Furuta, has a simple structure. A driven arm rotates in the horizontal plane and a pendulum attached to that arm rotates in the vertical plane. Theoretical modeling and the need to stabilize these movements are issues that have long racked the brains of engineers. With the Furuta pendulum, there are two variables: the direction of the rotational joint and that of the pendulum, which can be controlled. The pendulum is controlled in the vertical, unstable position, while the arm assumes any position. Since it is a nonlinear, unstable system, it is suitable for conducting experiments, for testing existing control algorithms, and for developing new calculation methods. It frequently combines approaches from research areas such as robotics, control theory, and computerized control.
 


Finding the right controller


A suitable controller can be developed using different design strategies. Suitable controller structures for an inverted pendulum include PID, LQR, fuzzy, or self-learning neural controllers. The physical system with multiple degrees of freedom can be modeled mathematically. For the swing-up of the pendulum from the rest position (zero position), nonlinear approaches such as energy approaches are required. A suitable controller is then designed with the help of the mathematical description. This controller can be approximated or discretized for real-time-capable systems and transferred to a controller such as the MiniMACS6-AMP4.




The compact controller


The maxon MiniMACS6-AMP4 is a programmable master controller with integrated power stages. It is the stabilizing controller for the rotational inverted pendulum. This allows complex movement patterns to be executed with simple commands, for example for jerk-free synchronization with a rotating master axis. Benefits of the MiniMACS6-AMP4 multi-axis controller:

  • Assumes the master function; no higher-level controller required
  • License-free motion control functionality included
  • Compact drive solution with integrated power stages

The license-free automation software ApossIDE (Integrated Development Environment) can be used to set up positioning and synchronization tasks with simple commands or you can run your own control algorithms using C (ApossC).#

MACS6_Control_Cascade_v2

Cascade control - Example of cascade control with a maxon motion controller such as the MiniMACS6-AMP4. The programmability and integrated path planning mean that a higher-level controller is not strictly required.



In action: The MiniMACS6-AMP4 stabilizes the rotational inverted pendulum.

 

COMPACT MiniMACS6-AMP4 multi-axis controller


The programmable multi-axis controller with integrated power stages is the stabilizing controller for the rotational inverted pendulum and ensures jerk-free synchronization with the rotating axis.


Latest issue


Read the current issue of maxon’s driven magazine featuring exciting stories, surprising facts and interesting technical articles on all aspects of drive technology. Discover it on our website: maxongroup.com/driven

Driven helping hands dt 1500x1000
Author: maxon HQ