maxon Story

Logistics robots in the ready-to-wear fashion

Topics

1a9a3369-0142f8ab1a9a3369-0142f8ab

C-Log, a subsidiary of the Beaumanoir Group, specializes in logistics for the retail and e-commerce sectors. With nine strategically located warehouses across France, the company not only ensures the seamless supply of stock to Beaumanoir's brands - Bonobo, Bréal, Cache-Cache, La Halle, Caroll, and Morgan - but also offers logistics services to other apparel labels.

When e-commerce really took off in 2019, C-Log decided to create a specific process to handle online orders. The result was an automated warehouse with 18,000 m2 of floor space, entirely dedicated to e-commerce, situated at Poupry, between Paris and Orléans. Built in 2022, this “Digital Hub” relies on a fleet of 240 autonomous mobile robots (AMR), capable of ensuring deliveries within 24 hours of an online purchase. Rather than procuring its robots from another country, the Beaumanoir Group took the somewhat daring risk of manufacturing them themselves, at Saint-Malo in Brittany. An instance of reshoring within a wider policy of genuine corporate social responsibility, and one which paid off. This is a story about robots, to be sure, but one in which humans are never far away.

c-log_poupry_00002-7d234d0e

Reshoring rather than offshoring: an unusual gamble with a great impact

The story began in 2019. Faced with rapid growth in its e-commerce business, C-Log was looking for a way to keep up and to get its rising costs under control. “The logistical costs of e-commerce are four times higher than those of in-store sales. The challenge was to break that four-to-one ratio for our customer brands,”, explained Benoît Garçon, CEO of C-Log. A request for proposals was sent out, with the Beaumanoir Group thinking of purchasing robots seen during earlier visits to other countries.

Julien Le Flohic and Georges Pagis, both with PhDs in robotics, had a different idea in mind. “We went to see Mr. Beaumanoir and suggested that he should manufacture the necessary robots for his warehouses in-house instead. It took a short PowerPoint to persuade him to invest in us, even though he didn’t know us! After an hour, his response was, ‘It’s awesome, I love it, where do I sign?’". As a well-informed entrepreneur deeply attached to his local region, he immediately took to the idea of robots made in Saint-Malo, recalled Georges Pagis, now technical director of C-Log’s robotics design department.

For the project to become a reality, a robotics design department was set up at C-Log, with an entrepreneurial outlook. Its mission? To manufacture mobile robots for use within the Digital Hub, before moving on to the automation and robotization of all the C-Log warehouses, with the aim of reducing the risks of musculoskeletal disorders inherent in repetitive tasks.

1a9a3396-411108df

“The Beaumanoir Group has always invested in logistics resources that can ensure availability of a product in the right store at the right time,” says Georges Pagis.

Three years later, in 2022, the Digital Hub was operational. This huge automated warehouse has the capacity to handle 40,000 items a day, with the most thorough system of automation possible. Enough to meet the many challenges of fashion retail logistics.

Digital Hub: ambitious goals

As well as decarbonizing and optimizing transport to limit its environmental impact, the ready-to-wear logistics industry faces various economic and human challenges. The Digital Hub was designed to meet these challenges.

  • Ensuring delivery in 24 hours. The first challenge concerns speed. No more than 24 hours should pass from the moment when a customer confirms their order online to the moment when they receive their order in the mail. To achieve that, it was critical that the Digital Hub is located near the hubs of the shipping carriers, to allow collection as late as possible.
  • Dealing with the proliferation of shipping carriers. Colis Relais, Mondial Relay, Colissimo, UPS, Fedex… There was once a time when only the postal service was tasked with delivering packages, but the number of carriers has since multiplied. This situation means that packages have to be sorted very carefully when they leave the warehouse, so that each is assigned to the right carrier.
  • Limiting manual handling of the garments by the human workers. In conventional warehouses, workers may be required to move more than one garment per second. Because such an intense pace can cause musculoskeletal disorders, one of the goals of the Digital Hub was to limit this kind of handling as much as possible.

“The usual practice in the past was to buy machines and then adapt their ergonomics to limit their impact. Now, people think about the process in advance, and about how everything is going to be done, so that everything is ergonomic. This allows arduous tasks to be minimized, thanks to automation and robotization. As a result, jobs are being displaced to positions of greater added value,” explained the C-Log robotics design technical director.

To address all of these challenges, C-Log has devised an innovative logistics process, based on a French and European registered patent.

1a9a3411-bis-0c11232c
c-log_poupry_00007-7cb85cb5
1a9a3411-bis-0c11232c
c-log_poupry_00007-7cb85cb5
1/2

Mobile robots and a gravity system: a world-first logistics system

Most robotics engineers working in logistics use the “goods to man” method, patented by Amazon. This method involves making the items in an order come to the pickers, who can then assemble the order. Robots bring the different components of the order to the stationary worker, so that the worker can put the order together.

«The logistics process that we have installed is truly the first of its kind in the world»

“We had a different idea about how to put the order together, by using our robots and a gravity system. The logistics process that we have installed is truly the first of its kind in the world, and we are very proud of it!” declared Georges Pagis.

In precise terms, as soon as an order is placed online, the items are removed from storage automatically by a network of conveyors on level 2. A stationary worker or a picking robot then picks up the garment and passes it to a mobile robot, which places it in an assembly area. Each robot carries only one garment at a time. In this way, the robots put the orders together and send them to packing and shipping, which have also been automated.

The entire process is managed by the control software, which assigns tasks in real time to the different robots according to the type of order.

vlcsnap-2023-06-13-13h06m38s512-955ebd69

“Thanks to the real-time workflow, we are able to send in orders throughout the day, thus distributing and smoothing out the workload. Ultimately, that means the pace can be reduced for the human workers, while also improving productivity,” explained the technical director of C-Log robotics design.

Whereas conventional materials handling facilities favor batch picking, in which batches of orders are picked at the same time, the Digital Hub works by picking the orders as they come in: After an order is placed on the website, it is processed in near-real time. “It’s the optimization and innovation of the processes that allows this change of model,” added Georges Pagis.

1a9a3543-2c48bed0

Robots costing half as much as those on the market

“The thing about our system is that, on the one hand, we have to move lightweight products, and on the other hand, a lot of robots are needed to make the process work, so there is a real need to minimize their costs,” stresses Georges Pagis. For this reason, it was necessary for the robots to cost as little as possible. In addition, the robotics design department at C-Log had to move fast, because the teams had less than two years to manufacture and deploy the robots in the Digital Hub. Two key factors were leveraged to meet these challenges:

  • Insourcing: Applying an agile methodology, the teams at C-Log did everything in-house, from the software development to the mechanical engineering, using a sprint system. A prototype was quickly constructed in order to collect data and improve the robot. The finished product is the end result of multiple iterations.
  • Modular design: This allowed each building block to be worked on independently: battery, motor system, intelligence, motherboard… Thanks to the modular nature of the design, as soon as one building block or module was functional, it was possible to go on to the next, without being held up.

“Maximized insourcing and the modular aspect allowed us to keep to very tight deadlines and to produce our first robots very quickly. In just two years, we produced 40 robots, manufactured completely in-house!” says Georges Pagis, whose team of 10 people has produced 200 more robots since.

“We have built robots lighter than what’s available on the market, by making modifications to all the components. That allowed us to get greater autonomy and a more attractive cost per robot than what exists on the market,” adds Gwendal Buzulier, director of product engineering at C-Log. When in the warehouse, the robots move around on a grid pattern equipped with QR codes. Every time a QR code is read, the central control system sends an instruction to the robot to keep it on track.

In the design, significant effort was also made to reduce the noise level of the robots, in order to ensure good working conditions in the warehouse.

maxon: a trusted partner for motor systems

When designing the motor system, the C-Log design department contacted several motor manufacturers, but it was maxon that immediately won them over. “Within the first six months, it was clear that we would work with maxon and they helped us understand our needs. They also very quickly provided us with the first prototypes for testing,” Georges Pagis recalled. Consequently, the motor module was able to be completed in record time, allowing the C-Log teams to spend their time on other modules.

The motor module has remained virtually unchanged since. “The C-Log team has an outstanding capacity for innovation. We’ve worked with them right from the start of their project, and we’re very happy that we can provide them with the technical solutions they need in order to reach their goals fast,” explains Christian Lucas, customer application engineer at maxon.

C-Log’s robots are fitted with two of maxon’s best-sellers: the EC-i 40 motors and the EPOS 4 controllers. Reliable, economical, and proven, these two technologies are available within 48 hours. The EC-i 40 brushless motors are particularly impressive in terms of:

  • Power density: The ratio of power to size allows the use of a compact motor
  • Energy efficiency: An important point for robots that run on batteries
  • Reliability: When used in the correct conditions, no EC-i 40 motor has ever broken down
eci40-8d30e844
epos4-51880324
eci40-8d30e844
epos4-51880324

EC-i 40

1/2

«It’s really the human support that maxon provides that makes the difference»

“We’ve been working with maxon for four years now and we have never had a breakdown, which is quite an amazing bonus. The technical and sales support is equally fantastic – Mr. Lucas and Mr. Tinant have really been very patient and very responsive right from the start, which is great! Beyond the reliability of the products, it’s really the human support that maxon provides that makes the difference,” states the C-Log robotics design technical director. And he adds: “If there’s the slightest problem, I get a straightforward technical response within an hour. If only all our suppliers were like that!”

“The C-Log teams have asked us for a lot of technical information over the last four years, and our exchanges have always been fluid and constructive and solution-oriented. Our relationship with them is very good. I think it must be a nice place to work,” confirmed Henri Tinant, automation engineer at maxon.

From now until 2024, C-Log plans to produce 500 more robots. The goal? To duplicate the system put in place at the Digital Hub, in order to use it in other warehouses or for other purposes. At the same time, the design department is working on the design of picking robots and on improving the conveyor system. It is also considering installing simple mechanisms to assist with actions likely to cause musculoskeletal disorders. To accommodate its ambitions, the C-Log design department is set to grow further, so as to support C-Log in automating its 10 warehouses. A marvelous endeavor, to which maxon is proud to contribute.

For more information: www.clog.fr

© by © maxon motor ag