maxon Story

Playing with water.

Topics

LKE_ExtremeMotionJet_41430_illustration-03LKE_ExtremeMotionJet_41430_illustration-03

maxon motor is renowned for its high-quality precision drive components. But customers often want more. A look at Germany, where maxon engineers work on complex complete solutions for gigantic water shows.

LKE_ExtremeMotionJet_ 41506-03
LKE_ExtremeMotionJet_41430_illustration-03
sexau
maxon_sexau_0046
EC45_flat_ECF_70W_9
hydrojet
LKE_ExtremeMotionJet_ 41506-03
LKE_ExtremeMotionJet_41430_illustration-03

EC 45 flat DC motors: The motors in the water jet are brushless EC 45 flat DC motors, which can supply 70 watts of power. They are energy-efficient and have a high torque.

1/6


The water fountains shoot up to 40 meters into the sky, drawing beautiful images, criss-crossing or forming parallel lines that harmonically swivel from side to side. Such water shows with dozens of fountains can be found all over the world: in the US, in Abu Dhabi, in China. Stationary or transportable. What they all have in common are high precision and attention to detail.


An unusual task


maxon is also about to dive into this waterworld. At the production site in Sexau, Germany, the engineers are developing an electrically controlled jet – lighter and more accurate than customary models. This is an unusual task for maxon. After all, as drive specialist, maxon is renowned worldwide for high-precision motors, gearheads, encoders and controllers. Yet in this case, maxon is delivering entire installation units of these water jets to the German customer LKE. In Sexau, everything comes together: engineering, manufacturing and as-sembly. “We have all the necessary expertise to offer such a complete solution in-house,” says designer Matthias Mamier. This is of advantage to the customer as it involves only a single contact partner who quickly implements his wishes and suggestions.

 

Motors completely immersed in oil


The short communication channels are beneficial when it comes to an application with high requirements. This also applies to the water jet. An example: All parts have to be made of stainless steel, so that they do not rust under water. Salty sea water must also not affect the unit. On the first floor at maxon, the mechanics machine the high-quality metal on CNC mills with micromillimeter precision. Here they create the cross manifold block, the heart of the water jet, so to speak. This work is no child’s play, as employee Lothar Scheerer tells us. “The high percentage of chromium in the metal requires a certain amount of experi-ence with machining it.”


The entire motion apparatus of the water jets is also quite sophisticated. It consists of two axles that are each moved by a motor-gearhead unit – completely immersed in oil. This makes it possible to operate the drives in overload, as the fluid has a cooling effect. How-ever, the oil must not leak out. Although it is biodegradable, it would discolor the water.


The drive itself consists of a brushless DC motor and a three-stage GP 42 planetary gear-head. The gearhead only has to travel a short distance. After all, maxon builds gearheads of all types in Sexau, from standard to special custom models (see box).

 

Electrical controller offers many advantages


For the past two years, maxon Sexau has been working on the development of the water jet. With the third generation of this product, the engineers have eliminated the last teeth-ing troubles: A new controller is able to compensate for an uneven position. This is useful when the jet is standing on the bottom of a lake. The seals of the oil-immersed drives have also been improved, plus the entire unit is now easier to assemble. Markus Diringer, who has assembled all prototypes hitherto, is particularly happy about this last benefit. “The water jets weigh 19 kilograms, so any simplification of the assembly procedure is very welcome,” he says, laughing.


Actually, the low weight is one of the big advantages of the electrically controlled water jets. Hydraulic models weigh around 80 to 90 kilograms each. They also need large, loud oil units. Electronic water jets make such units superfluous. And they offer more flexibility.


LKE wants to conquer the water show market with these advantages – and has found the right partner in maxon. A partner that is more than just a drive specialist. 

Author: Stefan Roschi